Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many auxiliary switches can be put in a Powerpact H or J Frame breaker?
Issue:
How many auxiliary switches can be put in a Powerpact H or J Frame breaker?

Product Line:
Circuit Breakers

Environment:
Powerpact H and J breakers

Resolution:
For a 3-pole breaker:
One or 2 auxiliary switch accessories can be added. Each is a 1A1B form C contact. This gives total 2A2B.
In addition, these breakers will accept one SD (alarm) switch and one SDE (overcurrent trip alarm) switch.
NOTE:  Installation of an SDx, NSX cord, BSCM, 24 Vdc Supply Terminal Block, or SDTAM accessory will affect the number of switches that can be installed.  See attachment for details.

An HD or HG 2-pole breaker will accept only one aux switch and one SD alarm switch.  An SDE is not possible.

Schneider Electric Canada

Attachment(s)
Placement of Switches.pdf [672.8 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings