How many starters can be connected via the GV2G454 bus bar?
Issue:
How many starters can be mounted on the GV2G### bus bar systems?
Environment:
Contactors and Starters-IEC
Product Line:
Tesys GV Manual Starter and Protectors
Resolution:
This will accommodate four GV2ME__ or GV2P__starters with one side mount auxiliary contact on each starter.
The GV2G**# part numbers contain this information in the part number. The ** indicates the pitch, while the # indicates the number of starters.
If ** is 54 there is 54 mm between the left side of one GV2 device and the next. ** being 45 indicates 45 mm and so on.
The # is the literal number of devices, 2 for 2 starters, 3 for 3 starters and so on.
Note: Cannot be used if GV2GH7 incoming line insulator.
How many starters can be mounted on the GV2G### bus bar systems?
Environment:
Contactors and Starters-IEC
Product Line:
Tesys GV Manual Starter and Protectors
Resolution:
This will accommodate four GV2ME__ or GV2P__starters with one side mount auxiliary contact on each starter.
The GV2G**# part numbers contain this information in the part number. The ** indicates the pitch, while the # indicates the number of starters.
If ** is 54 there is 54 mm between the left side of one GV2 device and the next. ** being 45 indicates 45 mm and so on.
The # is the literal number of devices, 2 for 2 starters, 3 for 3 starters and so on.
Note: Cannot be used if GV2GH7 incoming line insulator.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.