Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the dimensions of the Energy Efficent Transformers the same as the older standard units of the same voltage and temperature rating (such as a 112T3H)?
Issue:
Transformer Dimensions

Product Line:
Low Voltage Transformers

Environment:
Applies to LV Transformers

Cause:
Dimensional requirements

Resolution:


Energy Efficient Transformers have different dimensions than any  non-TP1 compliant units that they replace. If dimensions are critical, request a drawing to confirm.


CTA-ID : 2017151

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings