Issue:
8536 holding circuit
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Full Voltage Contactors and Starters
Resolution:
Terminals #2 and #3, additional information on terminations can be found within ``Device Terminal Identification`` instruction bulletin number 30072-007-85. This bulletin can be obtained via the Technical Library on the Intranet or from WWW.SQUARED.COM or simply by clicking on the link below.
8536 holding circuit
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Full Voltage Contactors and Starters
Resolution:
Terminals #2 and #3, additional information on terminations can be found within ``Device Terminal Identification`` instruction bulletin number 30072-007-85. This bulletin can be obtained via the Technical Library on the Intranet or from WWW.SQUARED.COM or simply by clicking on the link below.
Released for: Schneider Electric Canada