Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many Class 9999 Type AC04 auxiliary contact kits can be installed on the Motor Logic overload relay?
Issue:
Maximum Aux contact for Motor Logic overload relay

Product Line:
NEMA and Definite Purpose Contactor and Starter

Environment:
9065 Motor Logic overload relay

Resolution:
One 9999AC04 can be installed in the normally open or normally closed position. Note: This does not apply to Motor Logic Plus or Motor Logic Plus II overload relays as they are supplied as standard with a normally closed control circuit and normally open alarm circuit contacts as standard; no additional contacts are available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings