Issue:
Mechanical Operation ZB4/XB4 or ZB5/XB5
Product Line:
22 mm Push Buttons
Environment:
XB4 Specialty Operators
Resolution:
Mechanical operations for:
NOTE: Product life is based on average usage under normal operating conditions.
Mechanical Operation ZB4/XB4 or ZB5/XB5
Product Line:
22 mm Push Buttons
Environment:
XB4 Specialty Operators
Resolution:
Mechanical operations for:
- Push Button -- Spring return = 5 million, double headed = 1 million, push-push to release = 0.5 million
- Selector Switch -- non-illuminated = 3 million, illuminated = 1 million
- Toggle Switch = 0.5 million
- Emergency stop push button = 0.3 million
- Joystick = 1 million
- Standard blocks = 5 million
- Low power switching contact blocks = 0.5 million
- 1 million total electrical operations.
NOTE: Product life is based on average usage under normal operating conditions.
Released for: Schneider Electric Canada