Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the lugs on a NF18L1C and a NF418L1C the same?

Issue:
Main lugs used on a NF18L1C and a NF418L1C Panelboard

Product Line:
NF Panelboards

Environment:
Ordering

Cause:
Clarification

Resolution:
The Main Lugs are the same for Single and Three phase panelboards, just the quantities needed for each are different. For Both interiors, order lug part number 80114-312-50, with (3) needed for 3 phase, and (2) for single phase.

The mounting screws are part number 80114-001-01, (6) Screws needed for 3 phase and (4) needed for single phase.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings