Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the QO, 3-phase main lug ONLY (or FIXED main lug) load centers be converted to a main breaker load center?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO 3phase Load Center

Resolution:
ALL of the QO, 3phase Main lug load centers are considered FIXED Main Lug and CANNOT  be converted to a standard Main Breaker.


NOTE: the only option would be to back feed a branch breaker on the interior, BUT the branch breaker is limited to 100amp MAX and a retaining bracket kit is required. The branch breaker will require 3 pole spaces on the interior. ALWAYS FOLLOW WHAT THE National Electrical Code REQUIRES FOR BACK FEEDING AND SERVICE ENTRANCE.
1) If the Load Center will NOT be used as a Service Entrance panel the retaining kit part number is PK3MB.
2) If the load center will be used as a Service Entrance Panel the retaining kit part number is PKSB3BF.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings