Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Class 8538 Type S combination starters be supplied with DC control coils?
Issue:
Need to utilize DC control voltage in a Type S combination starter

Product Line:
NEMA and Definite Purpose Contactor and Starter

Environment:
NEMA combination starters

Resolution:
No, these starters use the Class 8536 Type S NEMA devices which are not available with DC control coils. You may use a DC controlled interposing relay and switch the contactor at line voltage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings