Issue:
Can the EDB breakers in a NF panels be used on 600Y/347V systems?
Product Line:
NF Panelboards
Environment:
Application
Cause:
Clarification
Resolution:
Yes, The NF panel and EDB breakers can be used for the 600V/347V Wye voltage system, as long as the 600v version of the EDB breaker is used, for example, p/n EDB36015.
This is contrast to the 480/Y277V rated EDB34015 breaker.
Can the EDB breakers in a NF panels be used on 600Y/347V systems?
Product Line:
NF Panelboards
Environment:
Application
Cause:
Clarification
Resolution:
Yes, The NF panel and EDB breakers can be used for the 600V/347V Wye voltage system, as long as the 600v version of the EDB breaker is used, for example, p/n EDB36015.
This is contrast to the 480/Y277V rated EDB34015 breaker.
Released for: Schneider Electric Canada