Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What field installable fuse blocks are offered for the 9070EO type Industrial Control Transformers?
Issue:
Fuse block options for EO Transformers

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Industrial Control Transformers may require fuse blocks

Resolution:

Fusing is only available for a single pole, typically used for secondary fusing, 30 amps maximum, glass type fuse.
The 9070AP3 is for the 25-150VA range.
The 9070AP4 is for the 200-750VA range.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings