Are larger main lugs available for the Homeline or QO load centers?
Issue:
Product Design Features
Product Line:
QO and Homeline Load Centers
Resolution:
QOL125VD will allow for (1) #4 - 2/0 AWG Cu wire or (1) #4 - 4/0 AWG Al wire and can ONLY be used in the Homeline, series S04 or higher and the QO, series S06 or higher, 125 A, single phase load centers marked appropriately on the wiring diagram in the accessory table.
EXCEPTION: Wire bending space does NOT permit use of aluminum wires larger than 2/0 AWG in the following load centers: QO120L125GC, QO120L125G, and QO12024L125G.
Product Design Features
Product Line:
QO and Homeline Load Centers
Resolution:
QOL125VD will allow for (1) #4 - 2/0 AWG Cu wire or (1) #4 - 4/0 AWG Al wire and can ONLY be used in the Homeline, series S04 or higher and the QO, series S06 or higher, 125 A, single phase load centers marked appropriately on the wiring diagram in the accessory table.
EXCEPTION: Wire bending space does NOT permit use of aluminum wires larger than 2/0 AWG in the following load centers: QO120L125GC, QO120L125G, and QO12024L125G.
Released for: Schneider Electric Canada