Issue:
Repalcement enclosure box or cover available for Class 2510 Type MBW or Type MCW NEMA 4 stainless steel or NEMA 4X glass-polyester
Product Line:
2510 type M manual starters
Environment:
Products sold and used in the United States
Cause:
Replacement enclosure needed for 2510MBW or 2510MCW
Resolution:
No, the complete enclosure which includes box and cover complete with external start/stop operator must be replaced. This applies regardless of the Series (A,B or C). Replacement enclosure is part number for stainless steel is 9991MW11, 9991MW1 for glass-polyester.
Update:
9991MW11 and 9991MW1 is already discontinued since 2021 without replacement.
Repalcement enclosure box or cover available for Class 2510 Type MBW or Type MCW NEMA 4 stainless steel or NEMA 4X glass-polyester
Product Line:
2510 type M manual starters
Environment:
Products sold and used in the United States
Cause:
Replacement enclosure needed for 2510MBW or 2510MCW
Resolution:
No, the complete enclosure which includes box and cover complete with external start/stop operator must be replaced. This applies regardless of the Series (A,B or C). Replacement enclosure is part number for stainless steel is 9991MW11, 9991MW1 for glass-polyester.
Update:
9991MW11 and 9991MW1 is already discontinued since 2021 without replacement.