Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a QOU14100JBAF?
Issue:
Product design features

Product line:
QOU Unit mount circuit breakers

Resolution:
The QOU14100JBAF is a front wired jumper bar assembly commonly used by OEMs. The device is rated 100 A, 240 VAC maximum. A neutral is not included. It accepts (4) poles of QOU circuit breakers (1 or 2 pole only), 60 A maximum. Each pole space must be filled. The device includes a base, cover, and mounting screw, but no enclosure. It carries a UR component listing and a CSA listing.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings