Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can You Field Convert the 9999SX Auxiliary Contact Modules?
Issue:
Information needed whether a type of auxiliary contact can be field converted from normally closed to normally open or normally open to normally closed

Product Line:
Contactors and Starters

Environment:
Type S Accessories and Components

Resolution:
Class 9999 Type SX6, SX7, SX8, SX9 and SX10 modules are field convertible.
Class 9999 Type SX11, SX12, SX13, SX14, SX15, SX16 and SX17 modules are not field convertible.

Schneider Electric Canada

Attachment(s)
30072-013-21.pdf [165.03 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings