Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Square D offer a 30mm 9001K control station rated for use in hazardous locations?
Issue:
What enclosures and operators to use for Class 1 Div 2?

Product Line:
30mm Push Buttons

Environment:

Type K and SK Electrical Components

Cause:
Determine is Schneider Electric has an control station to offer for this application.

Resolution:
Yes , but only for Class 1 Division 2 or Class II Division 2 Groups E & F.  Any Nema 4 & 13 enclosure ( ie. 9001KY** , KYSS** , SKY*** ) can be used,  if hermetically sealed contact blocks ( ie. 9001KA41 , 51 ) are used with 9001K or SK operators ( except potentiometers ) .

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings