Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is catalog number S106 for the QO or Homeline load centers?
Issue:
Product features

Product Line:
QO and Homeline Load Centers

Resolution:
The catalog number S106 is a package of 6 QO and Homeline load center cover screws. The S106 is sold ONLY through the retail channel with packaging that is a hanging type "Blisterpack", to allow a retailer to hang the package on a hook. The package consists of (6) 4020513002 (3/4" long) load center cover screws. Distributors should order cover screws as catalog number 4020513002K (3/4" long) or 4020513001K (1/2" long), which is a bag of 10 cover screws without the retail packaging.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings