Issue:
What operating mechanisms are compatible with the H and J frame circuit breakers?
Product line:
Circuit breaker operating mechanisms
Environment:
Class 9422 breaker operating mechanisms
Resolution:
The following are available:
Cable operators; 9422CSF30 (36 inches), 9422CSF50 (60 inches), 9422CSF70 (84 inches) & 9422CSF10 (120 inches).
Shaft driven; 9422RQ1.
NOTE: 9422A1 or 9422A2 Style flange handle must be purchased separately.
What operating mechanisms are compatible with the H and J frame circuit breakers?
Product line:
Circuit breaker operating mechanisms
Environment:
Class 9422 breaker operating mechanisms
Resolution:
The following are available:
Cable operators; 9422CSF30 (36 inches), 9422CSF50 (60 inches), 9422CSF70 (84 inches) & 9422CSF10 (120 inches).
Shaft driven; 9422RQ1.
NOTE: 9422A1 or 9422A2 Style flange handle must be purchased separately.
Released for: Schneider Electric Canada