Issue:
Need to know how many expansion modules can you use on the SR3 relays
Product Line:
Relays and Timers
Environment:
Zelio Logic Smart Relay
Resolution:
Depends on the type of the extension module:
The SR3** is capable of adding 1 I/O or 1 analog extension module along with 1 Modbus or Ethernet communication module.
A SR2COM01 communication module for the modem can also be connected to SR3** relay through the front port.
Need to know how many expansion modules can you use on the SR3 relays
Product Line:
Relays and Timers
Environment:
Zelio Logic Smart Relay
Resolution:
Depends on the type of the extension module:
The SR3** is capable of adding 1 I/O or 1 analog extension module along with 1 Modbus or Ethernet communication module.
A SR2COM01 communication module for the modem can also be connected to SR3** relay through the front port.
Released for: Schneider Electric Canada