Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do PowerPacT MG and MJ type breakers have a test port on the trip unit for secondary injection testing?
Issue:
Does MG and MJ type breakers have a test port on the trip unit for secondary injection testing?

Product Line:
Legacy Breaker

Resolution:
The PowerPacT M frame breakers have a perforated label over the test port. The perforation can be removed for access to the port. If the FFTK has the 1.10 version firmware or higher, it can be used to test the trip unit.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings