Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the bulbs be replaced in a XVDLS Tower lights?
Issue:
What is the replacement bulb for XVDLS34

Product Line:
Signalling Unit Monolithic tower lights

Environment:
Harmony® type XVD LS Ø 45 mm

Resolution:
There are 2 types of beacons and two types of light source available in XVDLS.
Beacon with steady light signalling operating with an incandescent bulb, 5w max and 230V max (to be ordered separately).

Bulbs for beacons with steady light signalling:
Incandescent bulbs BA 15d base fitting24V 4WDL1BEBS
120V 5WDL1BEGS
230V 5WDL1BEMS

Beacons with intermittent light fitted with 1 joule "flash" discharge tube (light source included).  No sold separately, need to replace the whole unit.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings