Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the contactor be replaced on the Class 8536 Type SE__ Nema Size 3 starter ?
Issue:
Replacement contactor needed for NEMA size 3 starter

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement contactor needed

Resolution:
No, the contactor busbars which mate up to the busbars on the overload are staked into the lower housing of the contactor. These busbars cannot be field added to the contactor. The baseplate will also be incorrect.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings