Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In safety switches that come with a solid neutral assembly, is it a switched neutral?
Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches

Resolution:
No, the solid neutral assembly does not switch the neutral.

NOTE: There are applications where a neutral conductor in a voltage system can be connected to one of the switching poles in a safety switch, BUT that is totally dependent on the application and the installer of the safety switch.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings