Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an RC1624M100S, Series M01?
Issue:
Repair parts list for RC1624M100S, series M1

Product Line:
CSEDs

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056172350 (includes latch)
Load Center Cover - 7329401401
Load Center Cover Hinges - (2) X2983
Load Center Cover Hinge Mounting Screws (2) 2159414081
Dead Front Interior Trim - 4056168402
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one is required)
Load Center Interior - 4056170150 (main breaker not included)
Load Center Interior Mounting Screws - (9) 2153217161
Main Breaker - HOM2100
Meter Base Assembly - 4056223250 (includes meter base with the right, load side meter jaw, blade guide, and L-shaped connector assembled to the meter base)
Meter Jaw - (3) 7329794850 (fourth is included in the meter base assembly, noted above)
Meter Jaw Mounting Bolt - (3) 2271020242 (fourth is included in the meter base assembly, noted above)
Meter Jaw Mounting Keps Nut - (3) 2342702001 (fourth is included in the meter base assembly, noted above)
Meter Jaw Blade Guide - (3) 4052761901 (fourth is included in the meter base assembly, noted above)
Line Side Phase Lugs - (2) 4025102451
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Line Side Neutral Lug - LK100AN
Closing Plate - (2) ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings