How can we help you today?

What are the repair parts for a QC2442M200C, series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (includes latch)
Load Center Cover - 4056157550 (includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056208001
Dead Front Interior Trim Mounting Screws - 4020513001K (this kit contains 10 screws; only 3 are required to mount the interior trim)
Dead Front Interior Trim Mounting Bracket - 4056162601
Dead Front Interior Trim Mounting Bracket Mounting Screw - 2142717480
Load Center Interior - 4056207750 (does not include main breaker)
Load Center Interior Mounting Screws - (6) 2153217161
Main Breaker - QOM2200VH, Mounting Hardware - (2) 2342702001 Keps Nuts
Meter Base Assembly - 4056190150 (includes meter base, line side lugs, line and load side meter jaws, line and load side meter jaw blade guides, and load side connector bussing)
Meter Jaw - (4) 7329794850 (included in meter base assembly)
Meter Jaw Mounting Keps Nuts - (4) 2342702001 (included in meter base assembly)
Meter Jaw Blade Guide - (4) 4052761901 (included in meter base assembly)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.