Issue:
Identify the terminals of the LC1F contactor
Product Line:
IEC Contactors and Starters
Environment:
TeSys F Contactors
Resolution:
The ``A1`` and ``A2`` terminals are for the coil voltage. The ``03`` and ``04`` terminals (if used) are a normally open auxiliary contact used for the holding circuit in three-wire control system for the LC1F115 through LC1F630.. contactor
Identify the terminals of the LC1F contactor
Product Line:
IEC Contactors and Starters
Environment:
TeSys F Contactors
Resolution:
The ``A1`` and ``A2`` terminals are for the coil voltage. The ``03`` and ``04`` terminals (if used) are a normally open auxiliary contact used for the holding circuit in three-wire control system for the LC1F115 through LC1F630.. contactor
Released for: Schneider Electric Canada