Issue:
Are there any single phase IEC motor starters?
Product Line:
Tesys contactors and motor controllers
Environment:
IEC Contactors and Starters
Cause:
Single phase motor starter needed
Resolution:
Yes. The customer could use a three phase contactor with an overload without single phase sensitivity. The U-line devices also have a single phase control module available.
Are there any single phase IEC motor starters?
Product Line:
Tesys contactors and motor controllers
Environment:
IEC Contactors and Starters
Cause:
Single phase motor starter needed
Resolution:
Yes. The customer could use a three phase contactor with an overload without single phase sensitivity. The U-line devices also have a single phase control module available.
Released for: Schneider Electric Canada