Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Could the obsolete Integral starter be used for single phase applications?
Issue:
Checking if the integral starters could be used for single phase applications.

Product Line:
Integral Starters

Environment:
Obsolete products

Resolution:
Due to single phase sensitivity of the protection modules, Integral Starters are designed for three phase applications. However, the overload module does not monitor phase angles. In a single phase application, the customer can wire 2 poles in series for one side of the load with the other side of the load returning thru the remaining pole.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings