How can we help you today?

What are the repair parts for a QU816D400FL, series M01?

Product Line:
CSEDs

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056236050 (one piece, meter cover/utility pullbox cover)
Meter Cover Mounting Wing Nuts - (4) 2350102000 and (1) sealing screw X1299
Load Center Cover - 4056258950
Load Center Cover Mounting Screws - (3) 2142217101
Load Center Interior - 4056259350
Load Center Interior Mounting Screws - (4) 2142217101
Load Center Interior Lugs - (2) 4025116051 and keps nuts (2) 2342702000
Interior Deadfront Trim - 4056233101
Interior Deadfront Trim Mounting Screws - 4020513001K
Meter Base Assembly - 4056257050
Mounting Channel - 4056142003
Factory Installed Main Breaker - QDL22200
Utility Lug Mounting Hardware - 4056211850
Semi-flush Flange Kit - FK400 (Includes top endwall, top flange, and two side flanges)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors