Issue:
Product Features
Product Line:
AC Disconnect
Resolution:
The line side terminal lug wire size is (1) #14 to #4 AWG Al/Cu and the load side terminal lug wire size (1) #14 to #6 AWG Al/Cu. The grounding terminal accepts (1) #14 to #8 Al/Cu.
Product Features
Product Line:
AC Disconnect
Resolution:
The line side terminal lug wire size is (1) #14 to #4 AWG Al/Cu and the load side terminal lug wire size (1) #14 to #6 AWG Al/Cu. The grounding terminal accepts (1) #14 to #8 Al/Cu.
Released for: Schneider Electric Canada