Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the auxiliary contact for a 9065 solid state overload relay ?
Issue:
Need an auxiliary contact for a 9065 solid state overload relay?

Product Line:
NEMA and Definite Purpose Contractors and Starters

Environment:
North American Products

Resolution:
This is the 9999AC04 module for Size 00 through 7 devices. It can be inserted into the overload in either the N.O. or N.C. status in a cavity underneath a removable flat black piece of Mylar above the overload contact terminals .

Note: Only one auxiliary contact block can be added

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings