Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can H, J, or L frame I-Line type breakers have interchangeable trip units?
Issue:
Can H , J or L frame I-Line type breakers have interchangeable trip units?

Product Line:
PowerPact H, J and L frame breakers

Resolution:
No. The interchangeable trip H, J, and L frame breakers are not available in I-Line configuration. They are available in unit mount only.
The I-Line mounting foot prevents the breakers from having interchangeable trip units.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings