Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CD224N, series F1? (may be shown as F01)
Issue:
Repair parts

Product Line:
Canadian General Duty Safety Switch

Resolution:
The replacement parts for the CD224N, series F1 (F01) are as follows. No other parts are available.
Complete Line Base -4056702950 (requires one line base per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020546401 (requires 6 per line base)
Load Base Assembly - 4056677450 (requires one per phase - includes phenolic base, lugs and fuse clips)
Load Base mounting screws - 4020546401 (requires 2 per load base)
Arc Suppressor Assembly - 4053922001(requires one per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678450
Switch Mechanism mounting screws - 2299940562 (requires 2)
Handle Assembly - 4056686250
Lockplate - 4056685701
Lockplate mounting screws - 2299940562 (requires 2)
Neutral Assembly - 4056678351
Neutral Bonding Screw - Contact (888) SQUARED for further assistance.
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings