Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the Class 8941 Duplex Motor Controllers UL listed?
Issue:
Are the Class 8941 Duplex Motor Controllers UL listed?

Product Line:
Class 8941 Duplex Motor Controllers

Environment:
Motor Starters

Cause:
Product Characteristics

Resolution:
The components are UL Listed, however, the 8941 as a complete unit is not UL listed unless it is ordered with Form Y1.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings