How can we help you today?

How to Set a 9050JCK On Delay Timer

Issue:
How to you set a 9050 type JCK On delay timer

Product Line:
9050JCK Timers

Environment:
Relays and Timers


Resolution:
The selection of the relay depends on the time interval and function mode for the application.  The dial on the top of the timer adjusts the time within this time interval. There is no specific time each notch corresponds to. The timing range will have to be by estimate.

Each specific timers have a timing range for minimum and maximum.

0.1–10 seconds for 9050JCK11
0.3–30 seconds for 9050JCK12
0.6–60 seconds for 9050JCK13
1.2–120 seconds for 9050JCK14
1.8–180 seconds for 9050JCK15
0.1–10 minutes for 9050JCK16
0.3–30 minutes for 9050JCK17
0.6–60 minutes for 9050JCK18
1.2–120 minutes for 9050JCK19