Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the field installation kit for a Hand-Off-Auto selector switch for Class 8502/8536 Type S controllers?
Issue:
What is the field installation kit for a Hand-Off-Auto selector switch for Class 8502/8536 Type S controllers?

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Field installing a hand off auto in a NEMA device

Resolution:
The field installation of factory Form C can be added based on the NEMA size and enclosure type as outlined below:

NEMA 1 Enclosure:
For NEMA sizes 00 through 3 = 9999SC2
For NEMA sizes 4 through 7 = 9999SC8

NEMA 3R and 12 Enclosures:
For All NEMA sizes = 9999SC8

NEMA 4/4X Stainless Steel Enclosures:
For All NEMA sizes = 9999SC9

NEMA 4/4X Poly Enclosures:
For All NEMA sizes = Not field installable.

Note: This applies to standard enclosures only, for oversized enclosures use the NEMA 3R and 12 selection data.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings