Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a CAFI (combination arc fault interrupter) circuit breaker merely a combination of an AFI breaker and a GFI breaker?
Issue:
Is a CAFI (combination arc-fault interrupter) circuit breaker merely a combination of an AFI breaker and a GFI breaker?

Product Line:
QO and HOM CAFI breakers

Resolution:
No, the CAFI (combination arc fault) breakers do not provide GFI level (6 mA) personnel protection.
"Combination" refers only to its rating for both parallel and series arc protection.

Arc fault and GFI personnel protection are provided by the DF (dual function) circuit breakers, however.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings