How do the accessory wires come out of a PowerPacT H, J, or L frame unit mount breaker?
Issue:
On the PowerPacT H, J, or L frame unit mount breakers, where do you run the control wire for accessories?
Product Line:
Circuit Breakers
Resolution:
For unit mount H, J, and L breakers, the accessory wires are routed through break-out tabs on the top edge of the breaker cover. The notches that define the tab locations are not always visible from the outside, while the cover is on the breaker. To see tabs, remove the breaker cover, turn it over, and look at the cover from the inside (see the picture). Use a pair of pliers to break out a tab. Then route the accessory wires through that opening and re-install the breaker cover.
On the PowerPacT H, J, or L frame unit mount breakers, where do you run the control wire for accessories?
Product Line:
Circuit Breakers
Resolution:
For unit mount H, J, and L breakers, the accessory wires are routed through break-out tabs on the top edge of the breaker cover. The notches that define the tab locations are not always visible from the outside, while the cover is on the breaker. To see tabs, remove the breaker cover, turn it over, and look at the cover from the inside (see the picture). Use a pair of pliers to break out a tab. Then route the accessory wires through that opening and re-install the breaker cover.
Released for: Schneider Electric Canada






Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.