Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement lugs for Class 8502/8536 NEMA Size 3, Type SE controllers?
Issue:
Identifying replacement lugs for NEMA size 3 contactor or starter

Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters

Environment:
North American Products

Cause:
Replacement lugs needed for NEMA Size 3 device

Resolution:
25050-94000 is the replacement power lug part number for either line side or load side. However, if lug mounting screw is also required it will be different as listed below:

8536:
Line side lug mounting screw: 21915-20200
Load side lug mounting screw: 21915-20140

8502:
Line and load side lug mounting screw: 21915-20200

Additionally, if control coil wire clamp is needed order part number 31051-007-50.

Please note all part numbers listed are for (1) piece, not complete replacement kits.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings