How can we help you today?

What are the replacement lugs for the 8502 SD size 2 contactor?

Issue:
Identifying replacement lugs for size 2 NEMA device

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement lugs needed for size 2 contactor

Resolution:
It is # 30016-018-50 for the lugs. Lugs come as a single unit. You will need 6 for a 3-pole device.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: