Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the largest branch circuit breaker that can be installed into a QO 3 phase load center?

Article available in these languages: Spanish

Issue:
Max amperage branch breaker that can be installed in 3-phase QO load center

Product Line:
QO Load Center

Resolution:
QO, 1 pole breaker maximum is 70 A.
QO, 2 pole breaker maximum is 125 A.
QO, 3 pole breaker maximum is 100 A.
NOTE: The maximum branch breaker cannot exceed the mains rating of the QO load center.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings