Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the mounting bracket for the Class 9999 Type SX Auxiliary Contacts available as replacement part?
Issue:
8502/8536 size 00-2 auxillary contact block mounting bracket

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Full Voltage Contactors and Starters

Resolution:
The mounting bracket is included with the auxiliary contact kit. However, if it becomes necessary to replace it order part number 31033-014-50. This bracket is only used on size 00 through size 2 devices.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings