Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a 8536SA NEMA size 00, 0, or 1 series A coil 31041-400-** be used in place of a 9998SAC** coil for the series B device?
Issue:
8536SA, SB, & SC A & B coils

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Magnetic Coils

Resolution:
No, the coils are not interchangeable. Using series A coils in series B starters will cause overheating.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings