Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the switching angle of the ZB5 XB5 selector switches?
Issue:
Needs to know the switching angle of the ZB5 XB5 selector switches.

Product Line:
Push Button and Operator Interface

Environment:
22 mm Push Buttons

Resolution:
Two position selector switches has a 90 degree angle.
Three position selector switches has a 45 degree angle.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings