Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does form DFJ2 indicate on the 8910DPA contactors?
Issue:
What is form DFJ2 on the 8910DPA contactors?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8910DPA Definite Purpose Contactor

Resolution:
Addition of a Class J 60 amp 600 volt (1 1/16 x 2 3/8 inch) 3 pole fuse holder. A fuse holder that mounted on top of the unit.  As an option, 9080FB3621J can be used and should be separate mounting.
Note: This factory modification is only valid on Class 8910 Type DPA13, DPA23, DPA33, DPA43, DPA53 or DPA63 contactors.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings