Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are EDB, EGB, and EJB breakers HID rated?
Product Line:
Circuit Breakers

Resolution:
1, 2, and 3 pole EDB, EGB, and EJB breakers from 15 A to 50 A are UL listed as HID (high intensity discharge) rated.
Breakers listed for HID will have the marking "HID" on the breaker itself. As an example, see the below picture.

Pic of breaker showing HID labeling

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings