Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of the forms M and M54 on busway products?
Issue:
Identify forms M and M54

Product Line:
I-Line Busway

Environment:
Products sold in North America

Resolution:
The M suffix indicates that the busway was designed to meet the drip resistant requirement in General Motor`s busway specification 13E.
The M54 suffix indicates that the busway was designed to achieve a IP54 degree of protection rating as defined by the International Standard IEC 529

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings