Issue:
Difference between the Series G contact block to the current Series of contact block.
Product Line:
Push Buttons and Operator Interface
Environment:
9001K/SK Heavy Duty Operators
Resolution:
The series G type terminal block does not have finger safe terminals and is used primarily when ring tongue or spade type terminals are used during wiring. All subsequent series numbers are finger safe and not compatible with those terminals. The series G type contact blocks are also 0.75" deep rather than the current 0.97" deep. Later series blocks have also been color coded and the normally closed contacts are positive opening.
Difference between the Series G contact block to the current Series of contact block.
Product Line:
Push Buttons and Operator Interface
Environment:
9001K/SK Heavy Duty Operators
Resolution:
The series G type terminal block does not have finger safe terminals and is used primarily when ring tongue or spade type terminals are used during wiring. All subsequent series numbers are finger safe and not compatible with those terminals. The series G type contact blocks are also 0.75" deep rather than the current 0.97" deep. Later series blocks have also been color coded and the normally closed contacts are positive opening.
Released for: Schneider Electric Canada