Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH361, series F5? (may be shown as F05)
Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repairt parts for the CH361, series F5 (F05) are as follows. No other parts are available.
Line Base Assembly -4056642050 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056002550K (1 required)
Arc Suppressor Assembly - 4056669451 (1 required) - Obsolete use part number NNZ56489
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Lockplate - 4056637601
Cover Latch - 40566-072-01
Latch Spring -  40223-043-01

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings