How can we help you today?

Are NEMA contactors offered with 2 normally closed and 2 normally open power contacts?

Issue:
Does Square D offer an 8502 contactor with 2 normally closed and 2 normally open power contacts?

Product Line:
NEMA Contactors

Environment:
Products sold and used in the United States

Resolution:
There are normally closed power pole adders available up to the NEMA size 2 offer, sizes 3-7 do not have an option for normally closed poles.
We can provide 2 normally open and two normally closed power poles with our (IEC Style) D-Line family of products up to the D80 contactors. See the IEC section of the Digest for details.
Also 2 normally open and 2 normally closed power poles are an option on Class 8910 DPA Definite Purpose contactors 20 amp inductive or 25 amp resistive through 40 amp inductive or 50 amp resistive contactors. See Class 8910 section of the current Digest for additional information.
NOTE: None of these solutions are recommended for use as a single phase transfer device.


Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings